Part Number: HD3SS3220
Can HD3SS3220 VDD5 pins support lower input power source of 3.8V to 4.3V where the power is from battery directly.
The VDD5 support internal pins power only, but I see no details blocks in datasheet.
I see ORT, ADDR, ENn_CC , CURRENT_MODE have Mid mode level, the datasheet share the range of VDD5 28% min,
but how much details voltage parameter these pins support? thanks.