This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1042-Q1: TCAN1042-Q1 VSON with lower consumption?

Part Number: TCAN1042-Q1
Other Parts Discussed in Thread: TCAN1043

hi Team,

customer checking for parts that be similar to TCAN1042-Q1 in VSON package and lower power consumption. 

please help recommend for such part.

Thanks

  • Hey John,

    I've assigned one of our enginners to take a look at this question. I suspect they will give you an answer by tomorrow.

    Thanks,
    -Bobby
  • Hi John,

    When operating in Normal Mode, the TCAN1042 performs at the same levels of power consumption as other TI device families:
    Normal Mode (dominant bit) = maximum 70mA
    Normal Mode (recessive bit) = maximum 2.5mA

    When operating in Standby Mode, the low power mode of the transceiver, then TI offers one device with lower VCC/VIO current than the TCAN1042. This device is the TCAN1044.

    TCAN1042 Standby Mode (VCC only) = maximum 22uA
    TCAN1042 Standby Mode (VCC/VIO) = maximum 5uA (VCC), maximum 17uA (VIO) [maximum 22uA total]

    TCAN1044 Standby Mode (VCC only) = maximum 12uA
    TCAN1044 Standby Mode (VCC/VIO) = maximum 1uA (VCC), maximum 11uA (VIO) [maximum 12uA total]

    The TCAN1044 is the lowest power 8-pin can device that TI currently offers. TCAN1044 is available in the 8-pin VSON package.

    You may also consider the TCAN1043, which is a 14-pin CAN solution that allows system-level power savings by offering Sleep Mode. Sleep Mode allows low quiescent power consumption at the transceiver level, but also provides an enable pin for the system-level power regulators. This means that the entire system may enter a low power mode when CAN traffic is not being processed.


    Do these recommendations help?

    Best Regards,
    Max Megee
    TI TRX Applications