Part Number: DS90UB954-Q1
HI
My customers are considering applying the DS90UB954-Q1.
However, when the test is performed at low temperature (-30 degree), the link is broken as shown in the waveform below.
Yellow: PASS
Blue: LOCK
Pink: POC 6.5V
Link drop time approx. 5ms
We do not see broken link when we test 6.5V power supply by connecting DC power supply after removing POC 6.5V power supply.
So we suspect the link broken due to POC power Noise. Noise of POC 6.5V power supply is 58mV pk-pk.
1. Is there a way to improve the problem by reducing the Noise by changing the Register for the above link breakage?
2. Is there any point to change POC block circuit and 954 peripheral circuit to improve noise?
3.What are the most important improvement points to improve this kind of thing (ex- circuit check and modification, PCB pattern check and modification, register change or etc...)
PS) If necessary, PCB pattern information can also be shared.
Please check it.
Thank you