This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS125MB203: cold sparing?

Part Number: DS125MB203

Is the DS125MB203 cold sparing?  I couldn’t see that in the datasheet.

  • Hello Michael,

    What is your definition of a device that can be a cold spare? I'm assuming, the device would need to have all I/Os high-impedance when VDD=0V? What would be the max Ioff leakage current requirement? Across what VIN range?

    Regards,
    Davor
  • At least the outputs or combined I/O channels should be at high impedance when the device is powered off.  This is most likely where the cold sparing capability will be needed.  Another definition would include all the inputs as well.  Another definition would include all the outputs, inputs, combined I/O, and control signals.  Leakage current would depend on the technology of the device and how good the chip designer is at getting it as low as possible.  I don’t believe there is any actual standard for maximum leakage current, other than it must have an insignificant effect on any device controlling the bus. 

  • Hello Michael,

    Like all high-speed interface devices, the DS125MB203 is exclusively intended for point-to-point connections. That is, there may only be a single TX driving a single RX over a transmission line. It is not recommended to have a second TX or RX (even as a cold spare) connected to the transmission line.

    Regards,
    Davor