This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90C385A: what's the max current of VCC, PLL VCC and LVDS VCC?

Part Number: DS90C385A


Hi 

in data sheet, there are the max current of VCC, PLL VCC and LVDS VCC, customer needs them, could you send me the data?

ICCTW is listed in datasheet, does this max current data is the maximum VCC current in all conditoions?

customer has an old version datasheet, the max TxCLKIN frequency is 85MHz, but in new datasheet on TI website, the max TxCLKIN frequency is 87.5MHz.

customer wants to know what's the reason caused this difference?

thanks.

  • Hi Max,

    We only have data for the total supply current, which is the Icctw you referenced. This is over recommended operating supply and temperature ranges.

    For the frequency, your customer probably has the datasheet for the DS90C385, which is different part number from the DS90C385A.

    Regards,
    I.K.