Hi,
Are there specific current draw specifications for all three rails in all modes. The data sheet appears to only show total power.
Thanks,
Mitch
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Are there specific current draw specifications for all three rails in all modes. The data sheet appears to only show total power.
Thanks,
Mitch
I am interested in characterizing currents for following modes:
RGMII to Copper (1G) (100m cable, 50% utilization)
RGMII to 1000Base-X (50% utilization)
1000Base-TX to 1000Base-FX (100m cable, 50% utilization)
Hi Mitchell,
Attached is the current consumption for the modes you requested.
| RGMII to Copper mode (100m cable, 50% utilization) | |||||||||
| Speed | VDDIO = 1.8V/3.3V | VDD2P5 = 2.5V | VDD1P0 = 1.0V | VDD1P8 = 1.8V | |||||
| V(V) | I(mA) | Power (mW) | I(mA) | Power (mW) | I(mA) | Power (mW) | I(mA) | Power (mW) | |
| 1000 | 1.8 | 17 | 30.6 | 88 | 220 | 119 | 119 | 52 | 93.6 |
| 1000 | 3.3 | 30 | 99 | 88 | 220 | 120 | 120 | 52 | 93.6 |
| RGMII to 1000Base-X (100m cable, 50% utilization) | |||||||||
| Speed | VDDIO = 1.8V/3.3V | VDD2P5 = 2.5V | VDD1P0 = 1.0V | VDD1P8 = 1.8V | |||||
| V(V) | I(mA) | Power (mW) | I(mA) | Power (mW) | I(mA) | Power (mW) | I(mA) | Power (mW) | |
| 1000 | 1.8 | 18 | 32.4 | 11 | 27.5 | 48 | 48 | 15 | 27 |
| 1000 | 3.3 | 32 | 105.6 | 11 | 27.5 | 48 | 48 | 15 | 27 |
| 1000Base-T to 1000Base-X (100m cable, 50% utilization) | |||||||||
| Speed | VDDIO = 1.8V/3.3V | VDD2P5 = 2.5V | VDD1P0 = 1.0V | VDD1P8 = 1.8V | |||||
| V(V) | I(mA) | Power (mW) | I(mA) | Power (mW) | I(mA) | Power (mW) | I(mA) | Power (mW) | |
| 1000 | 1.8 | 4 | 7.2 | 95 | 237.5 | 55 | 99 | 129 | 129 |
| 1000 | 3.3 | 9 | 29.7 | 95 | 237.5 | 129 | 129 | 55 | 99 |
Regards,
Hung Nguyen