Part Number: TUSB214
Other Parts Discussed in Thread: TUSB211, TUSB212
Hello
Below is customer topology and they just put TUSB214 on re-driver 2 position close to USB port and re-driver 1 short now. They test EQ level 0~level 3 of TUSB214 but eye diagram still cover the eye mask on below. Has any suggestion to pass eye diagram testing? Thank you.
|
CPU-->PCIE connector |
9 inch |
|
PCIE connector-->re-driver1 |
2 inch |
|
re-driver1-->re-driver2 |
10 inch |
|
re-driver2-->USB port |
10 inch |
EQ Level 3 :
EQ Level 0
BR
Patrick