Part Number: TUSB1064
Hi team,
My customer is using TUSB1064 in a product. The D+/D- pair of Type C connector is connected to MCU and the other signal lines of Type C connector is connected to TUSB1064.
Customer configures TUSB1064 to the USB3.1 mode and plugs the product to a laptop. But the laptop cannot recognize this product as a USB3.1 product. We also tried to configure TUSB1064 to the USB3.1+DP mode. But it cannot be recognized as USB3.1 either. We checked the USB cable and confirmed the cable is OK because laptop can recognize a USB3.1 cell phone through the same cable.
So do you have any advice on this issue?
What' s more, customer has below questions:
1. When TUSB1064 is powered up, what's the default mode without configuring any register? Is it default USB3.1 mode?
2. If we want to configure TUSB064 to DP 4 lanes mode, do we need to configure other register besides configuring 0x0a=0x02.
Thanks.
Best regards,
Wayne