Part Number: DP83867IR
Hi, In the DP83867 Troubleshooting Guide it is mentioned (no explicit mention of this in teh data sheet) that: "Each center tap of the magnetics should be independently de-coupled to ground via a 0.1uF capacitor." While it is quite easy to find RJ45 with magnetics having this option in big sizes ( I mean long 33mm) it is quite hard looking for shorter ones approx 22mm. There are RJ45s allowing for separate capacitors to center taps, however they also have all center taps shortened. Eg TE 1-2301994-2, link: www.digikey.co.uk/.../7516898 Could you please comment if such a jack is allowable and how the P1 should be connected? Thanks Sebastian