Part Number: ONET1151L
Hi,
I'm trying to understand the 85mA p-p MODulation current spec, coming up with two questions:
1.) Is the 85mApp MODulation current spec referring to that deliverable to an external (10-Ohm) load, or, referring to the internal diff pair sink itself ?
If the spec refers to the internal sink, it seems only half of the current (42.5mA) is available at the load.
2.) What is the voltage compliance at the MOD pin?
Thanks for your help