Part Number: TPS65987D
Hi TI,
I read the datasheet of TPS65987D. And have several questions as below.
1. What is the relationship between CC advertisement and configuration mentioned in Table7? For example, if I chose configuration 1 which set chip is DFP mode. But if another end I connect to a UFP, will device change the configuration after CC advertisement?
2.The datasheet says it can go up to 5A sink current. But there is no such a configuration in datasheet. Table7 on page 41 only support 3A sink current. Any other customized configuration can be supported?
3.Is the configuration of Table 7 saved in the chip or external SPI Flash?
4.If SPI flash can support more configuration, how can it be loaded to TPS65987D?
Our application needs to be a UFP, maximum power consumption will be around 20W.
Thanks!
cheers
Fan