Part Number: DS100BR111
Other Parts Discussed in Thread: DS64BR111, DS25BR120, DS25BR100, DS25BR110
Hi Guys
Can our DS100BR111 device support SGMII redriver? How determine which type of protocol interface we can support?
I just see the SGMII 1.25Gbps and only need two I/O port(RX and TX); Our device also has two pair differential ports(RX and TX)10Gbps. So I think it can support this. But not sure whether it is correct by using this parameters.
Your feedback are very appreciated.
Thanks
-Pengfei