Part Number: TUSB8041
Dear sir/madam,
I am using type 6 Intel based com express module and TUSB8041 usb hub on my baseboard. I have made upstream connection between type6 and usb hub as follows:
Vbus(type6) -> Vbus(hub);
D+(type6)->D+(hub);
D-(type6)->D-(hub);
Tx+(type6)->Tx+(hub);
Tx-(type6)-> Tx-(hub);
Rx+(type6)->Rx+(hub);
Rx-(type6)->Rx-(hub).
Is the connections right? or Should I connect Tx(type6 pair) to Rx(hub pair) and Rx(type6 pair) to Tx(hub pair)?