Part Number: HD3SS3220
Dear Sirs,
My customer use HD3SS3220 to design as DFP mode with attached schematics.
However, after testing, they found the mux cannot work well.
There is only one side(flip oriental) can be detected as USB3.0, other side always is USB2.0.
measured CC1/CC2/DIR and they are:
Pass: CC1=0.5V CC2=4.7V DIR=3.3V
Fail: CC1=4.7V CC2=0.5V DIR=3.3V
It seems the CC1/CC2 detect is OK but mux did not work.
We also refer to DFP dongle reference design of below link,
http://www.ti.com/lit/ug/sllu237a/sllu237a.pdf
and found the TX/RX connection between 3220 to type-C receptacle connector / 3220 to USB host are different.
Is that the root cause for the issue?
Please help to give me some suggestion.
Thanks.