Part Number: TPD3S714-Q1
Hi Sir,
Could you please help to clarify below questions?
Thanks
(1) VBUS_SYS(PIN14/PIN15) is used as INPUT and VBUS_CON(PIN2/PIN3) is used as OUTPUT ?
(2) Is the VBUS path current direction flow from VBUS_SYS(PIN14/PIN15) to VBUS_CON(PIN2/PIN3) ?
(3) If VBUS_SYS is supplied from device internal 5V , and VBUS_CON is connected to 5V from another device via USB connector, is it ok ?