Part Number: TCAN4550-Q1
Dear TI,
I have a need to understand the possibilities of using CAN FD as a field bus protocol sending IMU data through a CAN controller and forwarded through a CAN to WIFI gateway to another CAN to WIFI gateway and onward to the slave device. After it exits the wifi bridge it travels to another CAN FD controller (this one receiving masterclock from main MCU for system time stamp). Then forward to another CAN FD Controller at the slave end (apparently the hardware this CAN ports connect to at slave end has a baudrate of 9600.
I can see you have the hardware to do it in classical CAN 2.0b. But I’m really hoping to take advantage of the time stamp synchronisation available in the CAN FD 64bit hardware. I’m led to believe the jitter is much lower and data processing + latency adjustment are better served with this hardware than the early classical CAN 2.0b.
The major concern is getting that CAN FD data stream effectively across the Wifi gateway (can you get a can FD wifi gateway, or do you have to wrap the CAN FD in a TCP/UDP wrapper to achieve the stable low latency signal?
If I could send a data stream from one controller node over the wifi bridge to another can FD node and on to the next node at the slave, the my vision would be complete.... unfortunately I’m not away if the HW is available to attempt this design.
Any information as to its possibility would be greatly appreciated.
Many thanks for your time.
Regards
Stu