This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS110DF410: CDR Status Register REG 0x02

Guru 19785 points

Part Number: DS110DF410

Hi Team,

We would like to know the detail about th register REG 0x02 [4:2].

I am understanding that when Bit [5:4] = 11'b, we can judge that CDR is locked.
To achieve lock, I believe Bit [3] is also required to be "1", which means enough number of bit transition had been met.

Customer is observing REG 0x02 = 0xD8 = 1101 1000. In this case, system successed to link-up.

REG 0x02 = 0xD8 shows CDR is locked, however, it shows there were not enough bit transition to acuire CDR lock.

Can this happen ? What would be the condition that this status output could occur ?

Best Regards,
Kawai