Part Number: DS90UB928Q-Q1
Hi,
It’s about Deserializer DS90UB928-Q1.
Customer would like to know this deserializer BIST mode patterns.
In spec, it mentioned patterns as below list:
See attached file #1
As for pattern #14, #15, #16, the following are my understanding. Could you help me to double confirm it if my understanding is right or not?
- #14: Custom color is that we can separately set R/G/B 8-bit data value to decide output pattern, for example: we can set register PGRS=0x32, PGGS=0x32, PGBS=0x32, and then the pattern will be gray32.
- #15: Checkerboard pattern is set by PGCTL register, there are 2 type we can use. One is 1pixel x 1pixel, another on is 8pixels x 8pixels. As below picture: See attached file #2,3


3.#16: VCOM pattern: such as below:
See attached file #4