Part Number: USB-C-PD-DUO-EVM
Other Parts Discussed in Thread: TPS65987D, TPS65987
Dear Sir/Mam,
I've bought recently the USB-C-PD-DUO-EVM, and tried to program it.
I use TPS6598x Configuration Tool V5.1 and every time I try to program the EVB (both "Binary->SPI Flash from Binary File" and "Device->Flash App Firmware to Device"), I've got the message "SPI Flash to Device failed verification".
Can it be related to offsets, which are required to be entered during flash programming?
(I tried to read them back from PCB, got an error, so used default settings of 0x2000/ 0x20000)
I tried 2 ways to obtain the firmware:
1. Found this link: https://e2e.ti.com/support/interface/f/138/p/760683/2811140?tisearch=e2e-sitesearch&keymatch=USB-C-PD-DUO-EVM#2811140 and got PSIL054Sink.bin/PSIL054Source.bin file from there.
2. Found another link: https://e2e.ti.com/support/tools/sim-hw-system-design/f/234/p/781696/2891347#2891347?jktype=e2e – containing .pjt project for tps65987d, used TPS65987_88_F707_10_06.bin as a base image and customized the resulting settings.
What am I doing wrong while programming?
What is the right way to get and customize the firmware?
Thanks a lot and
Best Regards,
Boris.