Part Number: TCA9406
Dear Specialists,
My customer is considering TCA9406 and has a inquiry.
I would be grateful if you could advise.
---
According to "10 Power Supply Recommendations" in the data sheet of TCA9406,
“To ensure the high-impedance state of the outputs during power up or power down, the
OE input pin must be tied to GND through a pulldown resistor and must not be enabled until VCCA and VCCB are
fully ramped and stable.
Is this mandatory?
Ensuring high impedance of output if not needed, can the OE pin be high?
The connection of the TCA9406 are both microcomputers.
The pins of the microcomputer are high impedance until the power supply is stabilized.
For this reason, I thought that there was no problem even if the output of TCA9406 was not high impedance.
---
I appreciate your great help in advance.
Best regards,
Shinichi