Part Number: TCAN330
Dear Team,
My customer is surveying CAN controller and CAN transceiver solutions for their CAN device.
Here are some requirements of CAN solution:
1. 1Mbps datarate (No need CAN FD)
2. Need to support SAE J1939 spec.
Now they prefer to choose TCAN33x series solution, but they have some questions below. Please help to advise.
1. TCAN33x is compliant with 11898-2, so it should be able meet SAE J1939. But do they need to choose a CAN controller which is compliant with SAE J1939 as well?
2. Once the CAN device is ready. How could they test its function and signal quality? Is there any test flow for the CAN product that I can share to the customer?
3. Is there any driver (for Linux) or sample code support?
4. Is there any risk that if they choose the CAN controller from another vendor but use TI CAN transceiver? Any compatibility problem?
Thank you.
Jim