Part Number: TLK2711-SP
Hi
I am using the TLK2711A in my previous design.
Problem is that now I was told that there is a chance that the clock source of the TLK (towards the GTX_CLK pin) can be powered off while the TLK is still under power.
At this point this mean the GTX_CLK will be left floating !
I saw in the datasheet there is no internal pull up/ down over this pin.
Is this a problem?
Luckily, I made a preparation (which I didn't populate so far) for a parallel (R in serial with C) termination at the GTX_CLK pin.
For a GTX clock of 100Mhz , can you please suggest which values I can use in the two (R+C) free pads I currently have on board in order to both terminate the clock properly and as well solving the GTX floating issue?
Thanks a lot
Amnon