Part Number: TUSB1064
Hi Team,
Customer uses TUSB1064 for type C application. The application can support HBR2, however, HBR3 cannot display.
experiment setup
1. The source is from PC through assignment E cable.
2. We changed two different assignment E cable. the result is negative.
3. We tried to change the registers 0x10 and 0x11 value from 0x00 to 0xFF. But it still in vain.
The distance from type C connector to TUSB1064 is 2cm.
The distance from TUSB1064 output to SOC is 5cm.
Questions:
1. please review layout and provide your comment.
2. Is there any swing or driving current to modify?
schematic and layout

BR,
SHH