Part Number: SN65176B
Dear all:
50PCS sample board, all of SN65176B damage,replce use others production batch, test ok! the below test impedance to gnd's contrast,if have good advices for the issue.thank you!
pin normal abnormal1 abnormal2 abnormal3
pin1 0,659 infinity infinity infinity
others pin's impedance is normal.
Abnormal IC, main board insert power, but don't press power up key,PIN4 votage is 1.8V, PIN8 votage is 0.8V, when press power up key, SN65176B smoke and damage.
Normal IC, main board insert power, but don't press power up key,PIN4 votage is 3.3V, PIN8 votage about is 0V, when press power up key, SN65176B normal operate.
MCU support 3.3V stand-by power to PIN4 and PIN8 5V don't power up when don't press power up KEY.the below is the sch.