Other Parts Discussed in Thread: TCA9517A
We use the TCA9617A buffer for connecting 2 PCBs at the outside world with our main PCB. Both PCBs contain a few I2C chips (total number of 3 for both PCBs together) and are connected by means of a ribbon cable with our main board at the same I2C bus (at the output of the TCA9617A buffer). The length of the cable for one board is around 0.5m and for the second board around 0.3m. The max I2C speed we use is 400kHz.
My question is what you would recommend here for the values of the pull resistors for SDA and SCL? Do you recommend to place pull ups at both side of the cables (e.g. 10k at the main board en 10k at both external PCBs so the total value will be around 3k3? Or would you recommend to use just one pull up resistor here at the main board? In our application the external PCBs will always be present here because our software checks if they are present and connected.
Best Regards
Chris van der Aar
Sr. Hardware Designer
NTS Systems Development
Eindhoven The Netherlands