My customer wants to use the TUSB551 in X86 board.The distance between CPU and interface is 35inch.
Since TUSB551 is a single-channel re-driver, it can only compensating the CPU TX --- TUSB551 --- Recevier socket
How do I assign a distance of 35 inches?
Put TUSB551 in the middle of the CPU and receiver?
Or
Put TUSB551 in the position close to the CPU, or in the position close to Receiver socket?