Part Number: DS90UB933-Q1
Hi,
I'm trying to convert 12-bit CMOS output from a sensor (RGGB bayer) to MIPI CSI2 (2 lanes hopefully). Do you have any SerDes products available that can accomplish this? I am expecting around a 75 MHz pixel clock.
Any suggestions will help.
Thank you,
JP
UPDATE:
My thought is to use the DS90UB933-Q1 CMOS input serializer and the DS90UB936-Q1 MIPI CSI-2 output deserializer.
1) Will this work?
I'll be using two control video signals. 1) Line valid (active high for active pixel data ONLY ) and Frame Valid (active high for active pixel data and horizontal blanking periods, but low for vertical blanking periods).
2) Will there be an issue connecting these to the HSYNC and VSYNC pins?
3) If it's not an issue, do these sync pins need to defined at any point (at the processor at the output?) so that the above definitions of the control pins are understood by the system?