This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD1471: Problem in communicating SN65HVD1471 transceiver with MAX14850 isolator

Part Number: SN65HVD1471


Hi, I met a problem when i tried to interface my SN65HVD1471 transceiver with MAX14850 isolator. Please refer to my connection below,

R(Transceiver) - INA1- OUTB1 - Rx(MCU)

Tx(MCU)          - INB1 - OUTA1 - D(Transceiver)

Transceiver differential pair

A - TX+

B - TX-

Y - RX+

Z - RX-

Between A and B, Y and Z i connected 120 Ohms . After this connection does not works, i loop back the connection between OUTB1 and INB1, now also it is not working. I also tried with I/O pins. Please point out my mistake.

  • Hello,

    Y and Z are the transmitter outputs. A and B are the receiver inputs. It sounds like you may have them swapped - can you please double check this?

    Regards,
    Max
  • This is my schematic. During hardware check, i loop back  D and R, it works. But when i loop back UART_tx and UART_rx, it won't work.

  • If it works when you loop back D to R then the connections from the UART to the isolator must be OK. (It should also work, then, if you loop back Y to A and Z to B; have you tried this?)

    When you loop back UART_tx to UART_rx, are both VccA and VccB of the isolator powered up? I'm wondering if side A might be active and driving a low level that may be interfering with the loopback data.

    Also, I noticed that these ports of the isolator are open-drain. I don't see a pull-up resistance on the UART_tx or UART_rx lines, though - is this implemented somewhere else on the schematic (or integrated into the MCU)?

    Regards,
    Max