Part Number: DP83867E
I am using DP83867 ethernet PHY in SGMII mode.
- On page 6 pin functions it is mentioned that SGMII_COP/CON clock signal will generate continuous 625MHz clock.
- On page 56 of the datasheet PHYCR register has SGMII enable (bit 11) and 125MHz speed enable (bit 4).
I wanted to generate 125MHz from the differential clock from pins SGMII_COP/CON. Which one of the statements is correct?