Part Number: DS125DF410
Hi Team,
We have following questions about DS125DF410 False Lock Detector function.
---------------------------------------------------------------------------------------------------------------------
[Questions]
Q1). Do we need to enable this function ? Which is your recommendation ?
Q2). What happens when False Lock Detector function is kept disabled ?
Q3). If this bit must be de-asserted (REG 0x2F [1] = "0"), please correct the "Table 2. Standards-Based Mode Register Setting table" in the datasheet page 14 (SNLS398H).
---------------------------------------------------------------------------------------------------------------------
For DS125DF410, the default register setting DISABLEs the "False Lock Detector" function, which REG 0x2F [1] = "1".
However, I found that the datasheet requests to ENABLE this function by changing this bit to "0".
In 7.4.4.2, the datasheet requires user to set REG 0x2F [1] = "0" from "1".
However, the following Standards-Based frequency setting table is not enabling this False Lock Detector function.
This is very confusing.
Which is your recommendation ?
Best Regards,
Kawai