Part Number: DS90UB953-Q1EVM
Hi Team,
I would like to confirm if estimation for required band width is correct with below use case.
- image size : 1920 x 1080
- 60fps
- Blanking rate = 1.1
- CSI Output format of Image sensor : Raw12
Required Data Bandwidth : 1920*1080*1.1*12 = 1.642Gbps (<3.42Gbps)
Is it correct?
I especially want to confirm whether "Raw12" format means "12 bits for 1 pixel".
Best regards,