Part Number: TIC10024-Q1
I'd like to use TIC10024-Q1 as 24 High side Switch Sensor.
According to Spec sheet , only 10 inputs allow High side Switch, but 14 inputs are used for Low Side Switch.
My plan is followigs.
1. Put 22kohm between each input and ground.
2.Set Wetting Current 0mA
3.Set THRES_COMP = 2.0V (for example)
4. Each input is connected to High side Switch (Switch's another terminal is connected to VBAT)
Will ths operation work well?
Looking forward comments.