This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS125MB203: USB3.1 with DS125MB203

Part Number: DS125MB203

This is an appendix to the related questtion...

Is the DS125MB203 usable as an USB3.1 switch ?

The correct answer is NO, it is not usable for USB3.1 the reason is: the DS125MB203 inputs are terminated and the USB3 interface chip looks for a termination on the SS lines to detect if there is a host connected.

With the result the interface chip sees always the termination of the DS125MB203 and try to communicate on this line (and don't cares if the is a host) and never fall back to USB2.0.

I hope this helps others

regards

Milan