This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD1S514: Current in VBUS_Power

Part Number: TPD1S514


Hi TI!

I am not sure how to understand your datasheet of the TPD1S514x:

On page 4 under Absolute Maximum Ratings it is stated that the maximum current from the LDO you provide in this component is 1 mA.

However, on page 7 on the description of the VBUS_POWER Circuit it says maximum 3 mA. You also have a graph on page 9 with a 3 mA load condition.

What is the maximum current that is allowed to be drawn from the VBUS_POWER pin? Is it 1 or 3mA?
And is it safe to operate close to the current limit of 3 mA? Or can the OVP function then no longer be guarantueed?