Part Number: TPD1S514
Hi TI!
I am not sure how to understand your datasheet of the TPD1S514x:
On page 4 under Absolute Maximum Ratings it is stated that the maximum current from the LDO you provide in this component is 1 mA.
However, on page 7 on the description of the VBUS_POWER Circuit it says maximum 3 mA. You also have a graph on page 9 with a 3 mA load condition.
What is the maximum current that is allowed to be drawn from the VBUS_POWER pin? Is it 1 or 3mA?
And is it safe to operate close to the current limit of 3 mA? Or can the OVP function then no longer be guarantueed?