Part Number: HD3SS3412A
Other Parts Discussed in Thread: HD3SS3411
Hi team,
can you help to find solution can have PCIe gen 1 LANE to 4 PCIE?
work like PCIE Gen 1 Extender
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: HD3SS3412A
Other Parts Discussed in Thread: HD3SS3411
Hi team,
can you help to find solution can have PCIe gen 1 LANE to 4 PCIE?
work like PCIE Gen 1 Extender
Hi Bonnie,
PCIe is inherently a 1:1 serial link. There are active protocol aware switches which can be used to manipulate and distribute the PCIe topology. TI does not make this type of component. Passive switches like the HD3SS3412A are used on PCIe to provide a passive mechanism to switch between 1:1 PCIe connections. Only one connection is possible at a time.
Are you asking to have a 1 lane PCIe link go to 4 different locations at the same time?
Regards,
Lee
hI Lee,
switch is ok, but looks like 3412 can only switch from 1 Lane to 2 devices?
I need 1 to 4.
Hi Bonnie,
How fast will this application need to work Gen1? Gen2 or Gen3?
It would be possible to cascade several switches together if the channel is short enough to handle the additional losses associated with the passive switch.
Regards,
Lee
Hi Bonnie,
I don't have a reference circuit, but at Gen1 there should not be a performance or bandwidth issue. You will need 3x 2:1 switches to make a 4:1 switch in each direction.
Here is a basic picture of the interface for a PCIe 1x-lane 2.5 Gbps solution. Only one path could be selected at a time and the solution would not be dynamic, it would need to be configured with SELECT logic at power-up and held constant. For this type of application each mux would need independent SEL control like the HD3SS3411.
Regards,
Lee