This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TPS65983B: TPS65983B UCM Driver issue

Part Number: TPS65983B

Tool/software: Code Composer Studio

Dears

May I ask you two questions about the TPS65983 driver?

1. The customer reported that there was an error message in the installation attachment driver, which cannot be installed at present. The customer reported that a tps65983.sys file was missing, may I ask whether this file can be provided?

2.Do you have UCM driver For Win 10 RS5 For WHQL? (because we want to test WHQL internally, we are afraid that RS4 will not be able to test it)