Part Number: SN75178B
Other Parts Discussed in Thread: SN75176B, THVD1500, THVD1551, , THVD1550
Hi,
We are planning to add a buffer for our Motor Encoder RS-422 signals. I am calculating maximum current consumption by this IC on the board. It's mentioned in the datasheet that supply current (No Load) when the output is enabled max current would be 70mA. In our application output of this buffer would go to a controller with 120 ohms termination resistor. I am assuming output current would be roughly 20-25 mA.
My question is: should I add the output load current to the supply current for total consumption? In my case, would it be around 70+25 = 95 mA?
Thanks.
--Saumya