This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB9261-Q1: Difference of Terminal status about firmware version

Part Number: TUSB9261-Q1
Other Parts Discussed in Thread: TUSB9261

About the terminal.

Before, during device reset, I was told about the terminal status (input / output and logic) immediately after reset release. Does the terminal status change depending on the FW version?

The terminal state I was told before is below figure.

(Supplement)
As a reason to worry about the FW version,
In the future, when the FW is updated, if the status changes, there is a concern that it may not be absorbed by the hardware side.