Part Number: MAX3243E
Other Parts Discussed in Thread: MAX3243
Hi,
I'm using MAX3243 to convert UART to RS232.
Usualy it works and i can measure on the TX of the MAX3243 -6[V], and when data is transmitted i can see the data (115200 bps) between -6 to +6 [V].
This was great!
But... suddenly sometimes I loose communication !
I measured the TX again (when the failure occured) and I see that the voltage level is 0[V], and when the data transmitted it changed between 0 to 4[V] (insted of +-6V). It's important to say that the waveform looks good (the same as before) but the voltage level different.
more info: I changed the MAX3243 to a new one and it was the same (sometimes work and sometimes not - the same effect of 0-4[V] data)
So my questions is:
1. Do you have an idea when and why (generally) the TX changed between 0 to 4 [V]?
2. Do you have any idea how to understand what is the source of the failure?