Part Number: DP83867E
Hi, we are using the DP83867E on our board, and we have noticed some strange behavior when we power-on while plugged in to a 10/100 switch.
If we are plugged into a switch at power up, we will not get a link. I noticed that in Configuration Register 4 (Address 0x0031) the PORT_MIRROR_EN bit was set to 1. If I cleared this bit a link was established.
However, I did not see this issue when I powered on without the board plugged in to a switch, or if it was plugged in to a gigabit switch. I know this mode is set by the strapping pins (particularly LED_0) on power up and reset, could it be an issue there? Not sure why plugging in to a switch would have an impact as the LED_0 pin should have an internal pulldown on it.
We currently have the LED_0 pin going to a FDME1024NZT FET that drives an LED. Any feedback on the current set up and would could be causing this issue would be appreciated!