Part Number: TS5USBC400
Hello,
Can you please help with below questions on TS5USBC400:
1. Can it be used for switching 1.8V signals as well ?
2. When is the FLT pin asserted ?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TS5USBC400
Hello,
Can you please help with below questions on TS5USBC400:
1. Can it be used for switching 1.8V signals as well ?
2. When is the FLT pin asserted ?
Thanks!
Hi Nitish,
1. When you say 1.8 V signal is this a common mode voltage or VIH =1.8V, single ended? In the second case, yes, but care should be taken to not exceed OVP threshold.
2. FLT is asserted during a OVP event. Please see Figure 16. Overvoltage Protection Waveform, 16 V for a visual description.