This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVS3301: SMAJ36CA compatibility

Expert 5120 points

Part Number: TVS3301

Dear Support Team,

Would you have any comparison table between our TVS solutions and the SMA family? specifically for the SMAJ36CA where the closest solution (TVS3301) seems a too short in term of Reverse Stand-off Voltage.

Do you confirm?

Are there any other limitations?

Regards,

  • TISL-

    Unfortunately the highest voltage surge device we have is the TVS3301 which has a 33 V Vrwm. If higher is needed, we cannot support those requirements. However, please note that many times 33 V is as high of voltage as needed and 36V is added as extra margin due to higher leakage currents. Since the TVS3301 has lower leakage, less margin is needed.

    For a comparison between the device, please see the following white paper: www.ti.com/.../slyy127

    Thanks,
    Alec