Part Number: TCAN1043-Q1
Other Parts Discussed in Thread: TCAN1043
Hello,
I have two topics regarding CAN bus failure detection.
1) Is TCAN1043 able to detect a short between CANH and CANL ? Measurements and datasheet seem to show that nFault-pin does not signal the short state. How is such a failure handled / detected by the system ?
2) In event of nFault going low because of CANL/H short to GND / VSUP, how is it cleared after removal of short ? It is not cleared automatically. What is the procedure the host MCU must perform ?
The EVM User Guide states:
Flag is cleared: If fault is not present for four consecutive dominant to recessive transitions or upon leaving normal mode
Datasheets states:
Flag is cleared: Upon leaving Normal mode
Thank you
Martin