Part Number: ONET1151M
Hi, I've been instructed that the ONET1151M will operate without a controller.
1.) What is the procedure to operate the ONET1151M without a controller ? We don't need EQ or any of the digital optimization right now, just the ability to toggle the input and get output.
2.) We've measured the operating input (DIN+, DIN-) common mode DC voltage to be +1.7V. Provided we drive the input with a device with the same +1.7V CM voltage, can the inputs be DC-coupled ?
Thank you for your assistance,
J