Part Number: TPS25740B
Other Parts Discussed in Thread: TPS65987D
Hi,
Testing the TPS25740B EVM straight out of the box with my typeC PD phone, I only see 9V/1.3A, whereas I can measure the full 9V/2A with a wall charger. The default config looks like it should be able to support 9V/2A, though I've also tried changing the J7/8 jumpers but nothing changed.
How can I support the full 2A?
Thanks
Michael