Part Number: DS90UB954-Q1EVM
Other Parts Discussed in Thread: ALP, DS90UB949-Q1, DS90UB940-Q1
Hi all,
we are trying to interconnect multiple system in order to feed the ti953 with an RGB stream coming from HDMI to CSI-2 converter.
the chain contains; HDMI/CSi-2 converter -> TI953 -> TI954 -> CSi2to HDMI Converter.
we configured the scripts under alp in order to pass RGB888 and we are wondering if it is the same thing as the default RGB that is natively supported by HDMI 1.4?
we see that the TI954 report resolution but we are not sure if it is correct or no; we are using 1920*1080 @ 60fps as input in standard RGB.
can you provide us with a script that reads the data from the ti953 input connector (the one on which is supposed to connect the daughter card) on RGB and get it serialized and sent to the ti954? so we can compare to ours maybe we are missing something.
thank you in advance.