Part Number: DP83867IR
Other Parts Discussed in Thread: AM3352
Hi team,
The customer is using two AM3352s and two DP83867IRs to set up the test system. The issue is that the link is not stable and iperf3 test speed is 89Mbps in 1000M full-duplex mode. We assume that the issue come from the clock synchronization. Could you please tell me if the clock synchronization between processor and phy is necessary?
From the TIDA, the system is shown below. Clock synchronization is realized.
The customer used NXP platform before and the system is shown below. It also needs the synchronization.
AM3352 and DP83867 system is shown below.
Could you please comment on this? Thanks a lot.
Best regards
Chen