Part Number: DS125DF1610
Sometimes for development/test purpose, you may want to have a 10GbE PRBS generator. How would you setup DS125DF1610 to generate these different PRBS patterns.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS125DF1610
Sometimes for development/test purpose, you may want to have a 10GbE PRBS generator. How would you setup DS125DF1610 to generate these different PRBS patterns.
Using a clock which is a harmonic of the data rate, we can use DS125DF1610 to generate different PRBS pattern.
In example below, we are using 644.53125MHz clock (10.3125E9/16) to generate 10.3125Gbps PRBS pattern. Differential clock output from the synthesizer is attached to the RXA0 differential input and TXA0 generates PRBS pattern. Any other channel - other than RXA0/TXA0 - can be used for this operation as well.
RAW FF 01 03 //enable channel registers
RAW FC 01 FF //select rxa0/txa0 quad 0 channel 0
RAW FD 00 FF
RAW 2F B6 FF //setup rate sub-rate for 10GbE
RAW 0A 0C 0C //reset device
RAW 0A 08 0C //release reset
RAW 30 03 03 //reg 0x30[1:0] = 2'b11 prbs31 , = 2'b10 prbs15, = 2'b01 prbs9, and = 2'b00 prbs7
RAW 79 00 40 //disable prbs checker
RAW 79 20 20 //enable prbs generator
RAW 30 08 08 //enable prbs digital clock
RAW 1E 80 E0 //select prbs path for the output mux
RAW 1E 10 10 //enable prbs serializer
RAW 09 20 20 //enable 0x1E[7:5] setting to take effect
RAW 0C 00 08 //disable sbt check
RAW 0A 0C 0C //reset device
RAW 0A 08 0C //release reset wait for 500ms
RAW 02 00 00 //read reg 0x02 0x02[4:3]=2'b11 this indicates cdr lock
Regards,,nasser