Part Number: TMDS171
Other Parts Discussed in Thread: TMDS181, TMDS181RGZEVM
Hi Team,
Please advise me resolving a problem I encountered.
I tried to enable Pre-emphasis through Eye Scan tool GUI but could not do it.
When I set Pre-emphasis (either 2dB or 5 dB) mode and applied Write All,
The indicator got back to no-Pre-emphasis.
I also tried it through register menu (Address 0x0c bit 1:0 are set to 11b) but
register value got back to 00b. I confirmed that I2C_EN pin was set to High on the EVM.
I also set the re-timer mode in all case from 250Mbps to 6Gbps.
The termination mode behaves as Pre-emphasis mode too.
Please let me know how to configure the device in Pre-emphasis mode through the GUI.
Mita